Read/Write |
Description |
Set and return the ON/OFF subset correction state. Learn more. |
VB Syntax |
corrMethods.CorrectionSubsettingState = value |
Variable |
(Type) - Description |
corrMethods |
CorrectionMethods (object) |
value |
(Boolean) True Turns subset correction ON False Turns subset correction OFF |
Return Type |
Boolean |
Default |
True (-1) |
Example |
corrMethods.CorrectionSubsettingState = True |
C++ Syntax
|
HRESULT get_CorrectionSubsettingState(BOOL *state); HRESULT put_CorrectionSubsettingState(BOOL state); |
Interface |
ICorrectionMethods2 |