Write/Read
About Phase Control

CouplePhasePortSettings Property


Description

Sets and returns whether to couple phase control settings (IFBW, Tolerance, Max Iterations).

 VB Syntax

phase.CouplePhasePortSettings(srcPort) = value

Variable

(Type) - Description

phase

A PhaseControl Object

srcPort

(Long Integer) Source port for which to make phase control settings.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

value

(Boolean) Coupling state. Choose from:

True - Couple phase control settings. The phase control settings from <port> are copied to the other phase-controlled ports.

False - Do NOT couple phase control settings. The phase control settings for each phase-controlled port are made independently.

Return Type

Boolean

Default

False

Examples

phase.CouplePhasePortSettings 1 = True ' Write

value = phase.CouplePhasePortSettings 2' Read

C++ Syntax

HRESULT get_CouplePhasePortSettings(long port, VARIANT_BOOL* pVal);

HRESULT put_CouplePhasePortSettings(long port, VARIANT_BOOL newVal);

Interface

IPhaseControl