Read-Write
About FOM

Coupled Property


Description

Sets and returns the state of coupling (ON or OFF) of this range to the primary range.

 VB Syntax

FOMRange.Coupled = value

Variable

(Type) - Description

object

An FOMRange (object)

value

(boolean) - State of coupling.

True - Couple range to primary range.

False - Do NOT couple to primary range.

Return Type

Boolean

Default

True

Examples

fomRange.Coupled = False 'this range is NOT coupled to the primary range.

coupl = fomRange.Coupled 'Read

C++ Syntax

HRESULT get_Coupled(VARIANT_BOOL *pVal)
HRESULT put_Coupled(VARIANT_BOOL pVal)

Interface

IFOMRange