The FOM Range object provides access to the properties and methods for configuring a specific Range for frequency offset measurements.
Get a handle to a FOM Range by specifying an item in the FOM collection.
The FOM range items are typically numbered as follows:
Primary
Source
Receivers
Source2 (if present)
Source3 (if present)
External devices can appear in the list of range names. Learn more.
Dim app as AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim ranges as FOM
Set ranges = app.ActiveChannel.FOM
ranges.item(2).Coupled = False
Method |
InterfaceSee History |
Description |
|---|---|---|
None |
|
|
Property |
Interface |
Description |
IFOMRange |
Sets and returns the state of coupling (ON or OFF) of this range to the primary range. |
|
IFOMRange |
Set the Continuous Wave (CW) frequency. |
|
IFOMRange |
Sets and returns the Divisor value to be used when coupling this range to the primary range. |
|
IFOMRange |
Sets and returns the Multiplier value to be used when coupling this range to the primary range. |
|
IFOMRange |
Returns the name of this FOM range object. |
|
IFOMRange |
Sets and returns the offset value to be used when coupling this range to the primary range. |
|
IFOMRange |
Returns the index number of the range within the FOM collection. |
|
IFOMRange |
Collection - Used to add segment sweep capability to a range. |
|
IFOMRange |
Sets or returns the start frequency of this FOM Range. |
|
IFOMRange |
Sets or returns the stop frequency of this FOM Range. |
|
IFOMRange |
Sets the type of range sweep. |
Note: Use the Start Power and Stop Power settings from the channel object.
Interface |
Introduced with VNA Rev: |
IFOM |
7.10 |