Write/Read
About Fixturing

DiffPortMatchState Property


Description

Turns ON or OFF 4-port differential port matching function. Must also set the fixture simulator function to ON using FixturingState Property.

 VB Syntax

fixture.DiffPortMatchState = value

Variable

(Type) - Description

fixture

A Fixturing (object)

value

(Boolean)

False - Turns differential port matching OFF

True - Turns differential port matching ON

Return Type

Boolean

Default

False

Examples

fixture.DiffPortMatchState = False 'Write

value = fixture.DiffPortMatchState 'Read

C++ Syntax

HRESULT get_DiffPortMatchState( VARIANT_BOOL *pVal)
HRESULT put_DiffPortMatchState( VARIANT_BOOL newVal)

Interface

IFixturing2