Write/Read |
About Fixturing |
Description |
Sets the Resistance value of the differential matching circuit. |
VB Syntax |
fixture.DiffPortMatch_R(portNum) = value |
Variable |
(Type) - Description |
fixture |
A Fixturing (object) |
portNum |
(Integer) Balanced (logical) port number. Choose from logical ports 1, 2, or 3. Learn more about logical ports. |
value |
(Double) Resistance value in ohms. Choose a value between -1E18 to 1E18. |
Return Type |
Double |
Default |
0 |
Examples |
fixture.DiffPortMatch_R(2) = 1e3 'Write |
value = fixture.DiffPortMatch_R(1) 'Read |
|
C++ Syntax |
HRESULT get_DiffPortMatch_R(short portNum, double *pVal) |
Interface |
IFixturing2 |