Write/Read
About Electrical Delay

ElecDistanceDelayUnit Property


Description

Sets and returns the units for specifying electrical delay in physical length (distance).   

 VB Syntax

meas.ElecDistanceDelayUnit = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(enum naDistanceUnit) Choose from:

0 – naDistanceUnit_Meter

1 – naDistanceUnit_Feet

2 – naDistanceUnit_Inch

Return Type

Enum

Default

0 – naDistanceUnit_Meter

Examples

meas.ElecDistanceDelayUnit = naDistanceUnit_Meter  'Write

edelay = meas.ElecDistanceDelayUnit 'Read

C++ Syntax

HRESULT get_ElecDistanceDelayUnit(tagNADistanceUnit *pVal)
HRESULT put_ElecDistanceDelayUnit(tagNADistanceUnit newVal)

Interface

IMeasurement11