Phase Measurement Accuracy


You can increase the accuracy of phase measurements by using the following features.

See Also

Port Extensions

Comparing the Delay Functions

Phase Control

Phase Coherent Measurements

Learn more about Phase measurements

Electrical Delay

Electrical delay is a mathematical function that simulates a variable length of lossless transmission line.

Use the electrical delay feature to compensate for the linear phase shift through a device. This feature allows you to look at only the deviation from linear phase of the device.

You can set the electrical delay independently for each measurement trace.

How to set Electrical Delay

Using Hardkey/SoftTab/Softkey

  1. Press Scale > Electrical Delay.

 

Electrical Delay dialog box help

Electrical Delay  Specifies the value of delay added or removed, in Time or Distance.  This compensates for the linear phase shift through a device. You can set the electrical delay independently for each measurement trace.

Velocity Factor  Specifies the velocity factor that applies to the medium of the device that was inserted after the measurement calibration. The value for a polyethylene dielectric cable is 0.66 and 0.7 for PTFE dielectric. 1.0 corresponds to the speed of light in a vacuum.

Velocity factor can also be set from the Port Extensions dialog and Time Domain Distance Marker Settings.

Softkey Display  Allows you to enter delay in either Time or Distance using the softkeys and Active Entry toolbar.

Delay Distance  Changes the value when the Delay Time or Delay Distance values are changed.

Distance Units  Select from Meters, Inches, or Feet.  The step size will not change automatically when this value is changed.

Media

Coax  Select if the added length is coax. Also specify the velocity factor of the coax.

Waveguide  Select if the added length is waveguide. Also specify the low frequency cutoff of the waveguide.

Cutoff Freq  Low frequency cutoff of the waveguide.

Learn about Electrical Delay (scroll up)

 

Phase Offset

Phase offset mathematically adjusts the phase measurement by a specified amount, up to 360°. Use this feature in the following ways:

How to set Phase Offset

Using Hardkey/SoftTab/Softkey

  1. Press Scale > Constants > Phase Offset.

 

Phase Offset dialog box help

Phase Offset Type a value or use the up and down arrows to select any value up to 360 degrees.

Learn about Phase Offset (scroll up)

Spacing Between Frequency Points (Aliasing)

The analyzer samples data at discrete frequency points, then connects the points, creating a trace on the screen.

If the phase shift through a device is >180° between adjacent frequency points, the display can look like the phase slope is reversed. This is because the data is undersampled and aliasing is occurring.

If you are measuring group delay and the slope of the phase is reversed, then the group delay will change sign. For example, the following graphic shows a measurement of a SAW bandpass filter.

 

 

Tip:  To check if aliasing might be occurring in a measurement, either increase the number of points or reduce the frequency span.