| Read-only | About Path Configurator | 
| Description | Returns an array containing the names of configurable elements. See a list of configurable elements and settings for various VNA models. | 
| VB Syntax | values = pathConfig.Elements | 
| Variable | (Type) - Description | 
| values | (Variant array) Variable to store the array of configurable elements. | 
| pathConfig | A PathConfiguration (object) | 
| Return Type | Variant array | 
| Default | Not Applicable | 
| Examples | elems=pathconfig.Elements | 
| C++ Syntax | HRESULT Elements( VARIANT* pElements ); | 
| Interface | IPathConfiguration |