Write/Read
About Fixturing

EnableSnPDataExtrapolation


Description

Turns ON and OFF SNP file extrapolation for both 2-port and 4-port embedding/de-embedding.

 VB Syntax

fixture.EnableSnPDataExtrapolation  = bool

Variable

(Type) - Description

fixture

A Fixturing (object)

bool

True - Turns Extrapolation ON

False - Turns Extrapolation OFF

Return Type

Boolean

Default

False

Examples

fixture.EnableSnPDataExtrapolation = True

value = fixture.EnableSnPDataExtrapolation 'Read

C++ Syntax

HRESULT get_EnableSnPDataExtrapolation(VARIANT_BOOL *pExtrap);

HRESULT put_EnableSnPDataExtrapolation(VARIANT_BOOL bExtrap);

Interface

IFixturing6