Write-only
About Error Correction

ErrorCorrection (Channel) Property


Description

Attempts to set error correction ON or OFF for all of the measurements on the channel. This setting may not be successful for some measurements because the Cal Set currently in place may not contain the appropriate calibration data. To read the error correction state for a measurement, use Error Correction Property.

 VB Syntax

chan.ErrorCorrection = value

Variable

(Type) - Description

chan

A Channel (object)

value

(boolean)

False - Turns error correction OFF

True - Turns error correction ON

Return Type

Boolean

Default

About Error Correction

Examples

chan.ErrorCorrection = True

C++ Syntax

HRESULT put_ErrorCorrection (VARIANT_BOOL bState)

Interface

IChannel7