| Write/Read | About Phase Control | 
| Description | Write and read the fixed phase value. Must not be logarithmic sweep type. | 
| VB Syntax | phase.FixedPhase(srcPort) = value | 
| Variable | (Type) - Description | 
| phase | A PhaseControl Object | 
| srcPort | (Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port | 
| value | (Double) Phase value in degrees. Choose a value between -360 and 360. | 
| Return Type | Double | 
| Default | 0 degrees | 
| Examples | phase.FixedPhase 1 = 15 ' Write | 
| value = phase.FixedPhase 2' Read | |
| C++ Syntax | HRESULT get_FixedPhase(long port, double* pVal); HRESULT put_FixedPhase(long port, double newVal); | 
| Interface | IPhaseControl |