Write/Read |
|
Description |
Specifies the FOM frequency range to use when performing calibration. |
VB Syntax |
pref.FrequencyOffsetRangeForCalComputations = value |
Variable |
(Type) - Description |
pref |
A Preferences (object) |
value |
(Enum as NACalFOMRange) - Choose from: 0 - naCalFOMRangeAuto - All other calibration situations. 1 - naCalFOMRangePrimary - Used for calibrating at the mmWave frequencies when NOT using a test set. Learn more. |
Return Type |
Enum |
Default |
naCalFOMRangeAuto |
Examples |
pref.FrequencyOffsetRangeForCalComputations = naCalFOMRangePrimary 'Write |
calPref = pref.FrequencyOffsetRangeForCalComputations 'Read |
|
C++ Syntax |
HRESULT get_FrequencyOffsetRangeForCalComputations(tagNACalFOMRange * val); HRESULT put_FrequencyOffsetRangeForCalComputations((tagNACalFOMRange val); |
Interface |
IPreferences10 |