Write/Read
About Receiver Leveling

FrequencyType Property


Description

Sets and returns the frequency range to use for receiver leveling. On the user interface, this is the "Receiver frequency is determined by:" setting.

 VB Syntax

RxLevel.FrequencyType(srcPort) = value

Variable

(Type) - Description

RxLevel

A ReceiverLeveling Object

srcPort

(Long Integer) Source port for Receiver Leveling.

Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port

value

(Enum) Frequency range. Choose from:

naAutoFrequency (0) - always uses the frequency range that is assigned to the measurement receiver.

naInputFrequency (3) - Mixer/Converter input frequency range.

naOutputFrequency (4) - Mixer/Converter input frequency range.

naReceiverFrequency (1) - FOM Receiver frequency range.

naSourceFrequency (2) - FOM Source frequency range

Return Type

Enum

Default

naAutoFrequency (0)

Examples

rxLevel.FrequencyType (1) = naAutoFrequency ' Write

value = rxLevel.FrequencyType 2' Read

C++ Syntax

HRESULT get_FrequencyType(long port, tagNAFrequencyType* pVal);

HRESULT put_FrequencyType(long port, tagNAFrequencyType newVal);

Interface

IRxLevelingConfiguration3