Write/Read |
About Frequency Range |
Description |
Sets or returns the frequency span of the channel. Sets or returns the frequency span of the segment. |
VB Syntax |
object.FrequencySpan = value |
Variable |
(Type) - Description |
object |
A Channel (object) |
value |
(double) - Frequency span in Hertz. Choose any number between 70 (minimum) and maximum frequency span of the analyzer. |
Return Type |
Double |
Default |
Full frequency span of the analyzer |
Examples |
chan.FrequencySpan = 4.5e9 'sets the frequency span of a linear sweep for the channel object -Write |
freqspan = chan.FrequencySpan 'Read |
|
C++ Syntax |
HRESULT get_FrequencySpan(double *pVal) |
Interface |
IChannel |