Frequency range is the span of frequencies you specify for making a device measurement.
Auto Tune (Option S9x09xxA/B, S9x090A/B only)
Span All Meas Bands (Option S93070xB, S9x070A/B Modulation Distortion only)
See other 'Setup Measurements' topics
How to set Frequency RangeYou can also make these settings and more from the Sweep Type dialog. |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
Note: When number of ports is greater than 12, changing sweep parameters takes long time due to the calculation for collection. In order to avoid this, the Sweep Type dialog box is displayed instead of entry. |
|
Either of the following pairs of settings determine the frequency range. The last value that you enter determines the X-Axis labels. For example, if you enter the Start and Span values, the X-Axis will show Center and Span labels. Start /Stop - Specifies the beginning and end frequency of the swept measurement range. Note: The start frequency at preset may not be the minimum value in full range. Note: The maximum frequency of M9808A, P50x8A is 54 GHz. However, the specification is applied up to 53 GHz. (The maximum frequency is 53 GHz for the units shipped with the A.13.70 and below. Re-calibration is required for upgrade.) Center /Span - Specifies the value at the center and frequency range. Either of the following settings determine the number of evenly-spaced data points across the frequency range. Points - Specifies the number of evenly-spaced data points across the frequency range. Learn more about Data Points. Step - Available ONLY in Linear sweep type. Specifies the frequency step size between evenly-spaced data points. Changes to this setting will cause the Points setting to adjust to the closest integer. Any 'remainder' will adjust either the Stop value or Span value depending on which is displayed on the X-Axis label. |
Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.
Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.
How to Zoom in a measurement window |
Notes
Zoom is NOT available for the following:
|
Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.
How to set CW Frequency |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
CW Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the VNA. |
The resolution for setting frequency is 1 Hz.
The frequency range of the VNA covers several internal frequency bands. The higher the frequency range of the VNA, the larger the number of bands. The source power to your DUT turns off as the stimulus frequency is swept through these band crossings. To learn more, see Power ON and OFF during Sweep and Retrace.
The listed frequencies in the following tables are the stop frequency of the specified band, and the start frequency of the following band.
You can download a VNA Band Structure Readout utility that lists the band crossings for your VNA.
Frequency band crossings are different for the following models:
N5241B and N5242B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
.396 |
24 |
12.00 |
|
1 |
.010 |
13 |
.500 |
25 |
12.80 |
|
2 |
.014 |
14 |
.628 |
26 |
13.51 |
|
3 |
.019 |
15 |
1.00 |
27 |
15.20 |
|
4 |
.027 |
16 |
1.50 |
28 |
16.00 |
|
5 |
.038 |
17 |
2.00 |
29 |
18.00 |
|
6 |
.053 |
18 |
3.20 |
30 |
19.04 |
|
7 |
.075 |
19 |
5.332 |
31 |
20.00 |
|
8 |
.105 |
20 |
6.00 |
32 |
21.30 |
|
9 |
.146 |
21 |
7.6 |
33 |
24.00 |
|
10 |
.205 |
22 |
8.5 |
34 |
26.50 |
|
11 |
.250 |
23 |
9.52 |
|
||
|
|
|
|
|
N5244B and N5245B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
.396 |
24 |
12.00 |
36 |
30.40 |
1 |
.010 |
13 |
.500 |
25 |
12.80 |
37 |
32.00 |
2 |
.014 |
14 |
.628 |
26 |
13.51 |
38 |
36.10 |
3 |
.019 |
15 |
1.00 |
27 |
15.20 |
39 |
38.08 |
4 |
.027 |
16 |
1.50 |
28 |
16.00 |
40 |
40.53 |
5 |
.038 |
17 |
2.00 |
29 |
19.04 |
41 |
42.00 |
6 |
.053 |
18 |
3.20 |
30 |
20.00 |
42 |
43.50 |
7 |
.075 |
19 |
5.332 |
31 |
21.30 |
43 |
45.60 |
8 |
.105 |
20 |
6.00 |
32 |
24.00 |
44 |
48.00 |
9 |
.146 |
21 |
7.60 |
33 |
26.50 |
45 |
50.00 |
10 |
.205 |
22 |
8.50 |
34 |
27.02 |
|
|
11 |
.250 |
23 |
9.52 |
35 |
28.50 |
|
|
N5247B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
.396 |
24 |
12.00 |
36 |
30.40 |
48 |
60.10 |
1 |
.010 |
13 |
.500 |
25 |
12.80 |
37 |
32.00 |
49 |
60.80 |
2 |
.014 |
14 |
.628 |
26 |
13.51 |
38 |
36.10 |
50 |
64.00 |
3 |
.019 |
15 |
1.00 |
27 |
15.20 |
39 |
38.08 |
51 |
66.80 |
4 |
.027 |
16 |
1.50 |
28 |
16.00 |
40 |
40.00 |
52 |
70.00 |
5 |
.038 |
17 |
2.00 |
29 |
19.04 |
41 |
40.53 |
|
|
6 |
.053 |
18 |
3.20 |
30 |
20.00 |
42 |
45.82 |
|
|
7 |
.075 |
19 |
5.332 |
31 |
21.30 |
43 |
48.00 |
|
|
8 |
.105 |
20 |
6.00 |
32 |
24.00 |
44 |
50.00 |
|
|
9 |
.146 |
21 |
7.60 |
33 |
26.50 |
45 |
53.00 |
|
|
10 |
.205 |
22 |
8.50 |
34 |
27.02 |
46 |
54.04 |
|
|
11 |
.250 |
23 |
9.52 |
35 |
28.50 |
47 |
57.30 |
|
|
N5241B and N5242B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
.396 |
24 |
8.50 |
|
1 |
Reserved |
13 |
.500 |
25 |
10.664 |
|
2 |
.014 |
14 |
.628 |
26 |
12.00 |
|
3 |
.019 |
15 |
1.00 |
27 |
12.80 |
|
4 |
.027 |
16 |
1.50 |
28 |
13.51 |
|
5 |
.038 |
17 |
2.00 |
29 |
15.40 |
|
6 |
.053 |
18 |
3.00 |
30 |
16.00 |
|
7 |
.075 |
19 |
3.20 |
31 |
18.00 |
|
8 |
.105 |
20 |
4.00 |
32 |
20.00 |
|
9 |
.146 |
21 |
5.332 |
33 |
21.328 |
|
10 |
.205 |
22 |
6.752 |
34 |
22.50 |
|
11 |
.250 |
23 |
8.00 |
35 |
24.00 |
|
|
|
|
|
36 |
27.00 |
|
N5244B and N5245B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
.396 |
24 |
8.50 |
36 |
27.008 |
|
1 |
Reserved |
13 |
.500 |
25 |
10.664 |
37 |
32.00 |
|
2 |
.014 |
14 |
.628 |
26 |
12.00 |
38 |
36.50 |
|
3 |
.019 |
15 |
1.00 |
27 |
12.80 |
39 |
40.50 |
|
4 |
.027 |
16 |
1.50 |
28 |
13.51 |
40 |
42.656 |
|
5 |
.038 |
17 |
2.00 |
29 |
15.40 |
41 |
43.50 |
|
6 |
.053 |
18 |
3.00 |
30 |
16.00 |
42 |
46.20 |
|
7 |
.075 |
19 |
3.20 |
31 |
19.00 |
43 |
48.00 |
|
8 |
.105 |
20 |
4.00 |
32 |
20.00 |
44 |
50.20 |
|
9 |
.146 |
21 |
5.332 |
33 |
21.328 |
|
|
|
10 |
.205 |
22 |
6.752 |
34 |
24.00 |
|
|
|
11 |
.250 |
23 |
8.00 |
35 |
26.50 |
|
|
|
N5247B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
6.75 |
24 |
32.00 |
1 |
Reserved |
13 |
8.00 |
25 |
40.00 |
2 |
.053 |
14 |
10.70 |
26 |
40.50 |
3 |
.175 |
15 |
13.50 |
27 |
42.70 |
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
6 |
1.000 |
18 |
19.00 |
30 |
50.00 |
7 |
2.000 |
19 |
20.00 |
31 |
54.00 |
8 |
3.000 |
20 |
21.30 |
32 |
60.00 |
9 |
3.200 |
21 |
24.00 |
33 |
64.00 |
10 |
4.000 |
22 |
26.50 |
34 |
67.00 |
11 |
5.330 |
23 |
27.00 |
35 |
70.00 |
N5221B and N5222B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
15.20 |
1 |
.010 |
13 |
16.00 |
2 |
.053 |
14 |
18.00 |
3 |
.175 |
15 |
19.04 |
4 |
.250 |
16 |
20.00 |
5 |
.500 |
17 |
21.30 |
6 |
3.20 |
18 |
24.00 |
7 |
6.00 |
19 |
26.50 |
8 |
7.60 |
||
9 |
9.52 |
||
10 |
12.00 |
||
11 |
13.51 |
N5224B and N5225B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
15.20 |
24 |
38.08 |
1 |
.010 |
13 |
16.00 |
25 |
40.53 |
2 |
.053 |
14 |
19.04 |
26 |
42.00 |
3 |
.175 |
15 |
20.00 |
27 |
43.50 |
4 |
.250 |
16 |
21.30 |
28 |
45.60 |
5 |
.500 |
17 |
24.00 |
29 |
48.00 |
6 |
3.20 |
18 |
26.50 |
30 |
50.00 |
7 |
6.00 |
19 |
27.02 |
|
|
8 |
7.60 |
20 |
28.50 |
|
|
9 |
9.52 |
21 |
30.40 |
|
|
10 |
12.00 |
22 |
32.00 |
|
|
11 |
13.51 |
23 |
36.10 |
|
|
N5227B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
15.20 |
24 |
38.08 |
36 |
66.80 |
1 |
.010 |
13 |
16.00 |
25 |
40.00 |
37 |
70.00 |
2 |
.053 |
14 |
19.04 |
26 |
40.53 |
|
|
3 |
.175 |
15 |
20.00 |
27 |
45.82 |
|
|
4 |
.250 |
16 |
21.30 |
28 |
48.00 |
|
|
5 |
.500 |
17 |
24.00 |
29 |
50.00 |
|
|
6 |
3.20 |
18 |
26.50 |
30 |
53.00 |
|
|
7 |
6.00 |
19 |
27.02 |
31 |
54.04 |
|
|
8 |
7.60 |
20 |
28.50 |
32 |
57.30 |
|
|
9 |
9.52 |
21 |
30.40 |
33 |
60.10 |
|
|
10 |
12.00 |
22 |
32.00 |
34 |
60.80 |
|
|
11 |
13.51 |
23 |
36.10 |
35 |
64.00 |
|
|
N5221B and N5222B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
6.752 |
1 |
.010 |
13 |
8.0 |
2 |
.053 |
14 |
10.664 |
3 |
.175 |
15 |
13.51 |
4 |
.250 |
16 |
15.40 |
5 |
.500 |
17 |
16.0 |
6 |
1.0 |
18 |
20.0 |
7 |
2.0 |
19 |
21.328 |
8 |
3.0 |
20 |
24.0 |
9 |
3.2 |
21 |
27.0 |
10 |
4.0 |
22 |
|
11 |
5.332 |
23 |
|
N5224B and N5225B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
6.752 |
24 |
32.00 |
1 |
Reserved |
13 |
8.00 |
25 |
40.50 |
2 |
.053 |
14 |
10.664 |
26 |
42.656 |
3 |
.175 |
15 |
13.51 |
27 |
43.50 |
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
6 |
1.000 |
18 |
19.00 |
30 |
50.20 |
7 |
2.000 |
19 |
20.00 |
|
|
8 |
3.000 |
20 |
21.328 |
|
|
9 |
3.200 |
21 |
24.00 |
|
|
10 |
4.000 |
22 |
26.50 |
|
|
11 |
5.332 |
23 |
27.008 |
|
|
N5227B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
12 |
6.752 |
24 |
32.00 |
1 |
.010 |
13 |
8.00 |
25 |
40.00 |
2 |
.053 |
14 |
10.664 |
26 |
40.50 |
3 |
.175 |
15 |
13.51 |
27 |
42.656 |
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
6 |
1.000 |
18 |
19.00 |
30 |
50.00 |
7 |
2.000 |
19 |
20.00 |
31 |
54.00 |
8 |
3.000 |
20 |
21.328 |
32 |
60.00 |
9 |
3.200 |
21 |
24.00 |
33 |
64.00 |
10 |
4.000 |
22 |
26.50 |
34 |
67.00 |
11 |
5.332 |
23 |
27.008 |
35 |
70.00 |
N5231B, N5232B, N5239B
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
Reserved |
10 |
5.33 |
1 |
.000425 |
11 |
6.75 |
2 |
.0012 |
12 |
8.00 |
3 |
.0075 |
13 |
10.07 |
4 |
.025 |
14 |
13.50 |
5 |
.050 |
15 |
16.00 |
6 |
1.00 |
16 |
16.70 |
7 |
2.00 |
17 |
20.01 |
8 |
3.00 |
|
|
9 |
4.00 |
|
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
0 |
|
11 |
10.66 |
21 |
30.80 |
1 |
.010 |
12 |
13.51 |
22 |
31.50 |
2 |
.250 |
13 |
15.40 |
23 |
32.00 |
3 |
.500 |
14 |
16.00 |
24 |
40.00 |
4 |
1.00 |
15 |
20.00 |
25 |
40.56 |
5 |
2.00 |
16 |
20.26 |
26 |
42.00 |
6 |
3.00 |
17 |
21.33 |
27 |
48.00 |
7 |
4.00 |
18 |
24.00 |
28 |
50.00 |
8 |
5.332 |
19 |
26.00 |
|
|
9 |
6.752 |
20 |
27.01 |
|
|
10 |
8.00 |
|
|
|
|
The Auto Tune softkey is a feature of the Spectrum Analyzer measurement class (Option S9x09xxA/B, S9x090A/B). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.
The Span All Meas Bands softkey is a feature of the Modulation Distortion measurement class (Option S93070xB, S9x070A/B only). Each time this softkey is pressed, all defined distortion measurement bands for the modulation channel are automatically tuned.