| Write-Read | About IO Configuration | 
| Description | Set and returns HiSLIP instrument number. | 
| VB Syntax | IOConfig.HiSLIPAddress = value | 
| Variable | (Type) - Description | 
| IOConfig | An IOConfiguration object. | 
| value | (Long) HiSLIP instrument number. | 
| Return Type | Long | 
| Default | 0 (which renders "inst0") | 
| Examples | IOConfig.HiSLIPAddress = 1 'Write value = IOConfig.HiSLIPAddress 'Read | 
| C++ Syntax | HRESULT get HiSLIPAddress(long Address); HRESULT put HiSLIPAddress(long * Address); | 
| Interface | IIOConfiguration |