Write-Read
About IO Configuration

HiSLIPPort Property


Description

Set and returns the TCPIP port for HiSLIP communication.

 VB Syntax

IOConfig.HiSLIPPort = value

Variable

(Type) - Description

IOConfig

An IOConfiguration object.

value

(Long) HiSlip port number.

Return Type

Long

Default

4880

Examples

IOConfig.HiSLIPPort = 4880 'Write

value = IOConfig.HiSLIPPort 'Read

C++ Syntax

HRESULT get HiSLIPPort(long port);

HRESULT put HiSLIPPort(long * port);

Interface

IIOConfiguration