Write/Read
About Ext Pulse Gens

HighAmplitude Property


Description

Sets and returns the High amplitude (voltage) of the pulse generator.

 VB Syntax

extPulseGen.HighAmplitude = value

Variable

(Type) - Description

extPulseGen

An ExternalPulseGenerator (object)

value

(Double) Pulse Generator high amplitude voltage.

Return Type

Double

Default

5

Examples

extPulseGen.HighAmplitude = 4 'Write

hi = extPulseGen.HighAmplitude 'Read

C++ Syntax

HRESULT get_HighAmplitude (double *pValue)

HRESULT put_HighAmplitude (double newVal)

Interface

IExternalPulseGenerator