Read-only
About Independent Power Calibration

IndependentPowerCalibration Property


Description

This property returns a handle to the IndependentPowerCalibration object.

 VB Syntax

calAll.IndependentPowerCalibration( )

Variable

(Type) - Description

calAll

A CalibrateAllChannels (object)

Return Type

IIndependentPowerCalibration

Default

Not Applicable

Example

CalibrateAllChannels.IndependentPowerCalibration()

C++ Syntax

HRESULT IndependentPowerCalibration( IIndependentPowerCalibration **obj);

Interface

ICalibrateAllChannels2