Read-only |
About Embedded LO |
Description |
Returns whether or not a marker was used for the specified tuning sweep. |
VB Syntax |
value = embedLODiag.IsMarkerOn (n) |
Variable |
(Type) - Description |
value |
(Boolean) Variable to store the returned data. |
embedLODiag |
An EmbeddedLODiagnostic (object) |
n |
Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken. |
Return Type |
(String) |
Default |
Not Applicable |
Examples |
data= embedLO.IsMarkerOn 3 'read |
C++ Syntax |
HRESULT IsMarkerOn(long sweep, VARIANT_BOOL* markerOn); |
Interface |
IEmbededLODiagnostic |