| Write/Read | About Mixer Configuration | 
| Description | Sets or returns the number of LO stages present in the mixer. | 
| VB Syntax | obj.LOStage = value | 
| Variable | (Type) - Description | 
| obj | A Mixer Interface pointer to the Measurement (object) Or | 
| value | (Long) - Number of LO stages. Choose from 1 or 2 | 
| Return Type | Long | 
| Default | 1 | 
| Examples | mixer.LOStage = 1 'sets the LO Stage value to 1 | 
| C++ Syntax | HRESULT get_LOStage(long *pVal) HRESULT put_LOStage(long newVal) | 
| Interface | IMixer IConverter |