| Write/Read | About Swept IMDx | 
| Description | Sets or returns the Stop value of a LO Power sweep. Also set imdx.SweepType to naIMDLOPowerSweep. | 
| VB Syntax | obj.LOStopPower (n) = value | 
| Variable | (Type) - Description | 
| obj | |
| n | (Long) - LO stage number. Choose 1 | 
| value | (double) - LO Stop power in dBm. | 
| Return Type | Double | 
| Default | -10 dBm | 
| Examples | convtr.LOStopPower(1) = -5 'Sets the LO Power sweep Stop value Stop = convtr.LOStopPower(1) 'Reads the Stop value | 
| C++ Syntax | HRESULT get_LOStopPower(long LOStage, double *pVal) HRESULT put_LOStopPower(long LOStage, double newVal) | 
| Interface | IConverter |