Write/Read
About External Testset Control

Label Property


Description

Sets or gets the display label for a given channel/testset combination. The label appears in a status bar at the bottom of the VNA display when the ShowProperties property is set to TRUE.

 VB Syntax

tset.Label(chNum) = value

Variable

(Type) - Description

tset

A TestsetControl object.

Obtained from the ExternalTestsets collection.

chNum

(Integer)  Channel number of the measurement.

value

(String) The text of the label.

Return Type

String

Default

None

Examples

'The following sets the label for channel 5 corresponding to a given testset object.

testset1.label(5) = 'High-power output'

See External Testset Program

C++ Syntax

HRESULT get_Label(long channelNum, BSTR *pLabel);
HRESULT put_Label(long channelNum, BSTR label);

Interface

ITestsetControl