Write/Read |
About DC Sources |
Description |
Sets and returns the Max DC limit value for a DC source. |
VB Syntax |
dc.LimitMax(deviceName) = value |
Variable |
(Type) - Description |
dc |
A DCStimulus (object) |
deviceName |
(String) Name of the "DC source" Use Source Property to read a list of configured DC source names. |
value |
(Double) Max DC limit value. Choose a value within the range of the DC source. |
Return Type |
Double |
Default |
10 |
Examples |
dc.LimitMax("myDCSource") = 10 'Write value = dc.LimitMax("myDCSource") 'Read |
C++ Syntax |
HRESULT get_LimitMax(BSTR deviceName, double* value); HRESULT put_LimitMax(BSTR deviceName, double value); |
Interface |
IDCStimulus2 |