When a DC Source (power supply) is configured as an external device, the new DC source can be controlled from the VNA using this dialog. Internal DC Sources are also controlled from this dialog.
Configure the DC Source as an External Device
Internal DC Sources - ADC Measurements
Other Setup Measurements Topics
Note:
The 9-pin PWR I/O (Power I/O)
D connector on the rear-panel replaces much of the functionality
of the AUX I/O connector on older VNA models. The Power I/O voltages
can be set using the following methods: Name Lists the names of the configured DC Sources. In the above image:
State Set the state of the DC source.
Start / Stop DC Set the start and stop voltages of the DC source. The VNA will step the voltage of the DC source from Start to Stop in increments = (Stop - Start)/Number of data points. ButtonsLimits Click to start the DC Limits dialog. Receiver Leveling For future use. |
Select the Minimum and Maximum voltages to which the specified DC sources can be set by the VNA. When the DC source level exceeds the limit, DC source is turned off and the measurement sweep stops.
|