| Write/Read | About DC Sources | 
| Description | Sets and returns the Min DC limit value for a DC source. | 
| VB Syntax | dc.LimitMin(deviceName) = value | 
| Variable | (Type) - Description | 
| dc | A DCStimulus (object) | 
| deviceName | (String) Name of the "DC source" Use Source Property to read a list of configured DC source names. | 
| value | (Double) Min DC limit value. Choose a value within the range of the DC source. | 
| Return Type | Double | 
| Default | -10 | 
| Examples | dc.LimitMin("myDCSource") = -10 'Write value = dc.LimitMin("myDCSource") 'Read | 
| C++ Syntax | HRESULT get_LimitMin(BSTR deviceName, double* value); HRESULT put_LimitMin(BSTR deviceName, double value); | 
| Interface | IDCStimulus2 |