Write / Read |
About Source Power CalAbout PMAR |
Description |
Sets or returns the loss value associated with a PowerLossSegment. |
VB Syntax |
lossSeg.Loss = value |
Variable |
(Type) - Description |
lossSeg |
A PowerLossSegment (object) A PowerLossSegmentPMAR (object) |
value |
(double) – Loss value in dB. Loss is entered as a POSITIVE number. |
Return Type |
Double |
Default |
0 |
Examples |
lossSeg.Loss = 0.5
'Write |
C++ Syntax |
HRESULT put_Loss(Double newVal); HRESULT get_Loss(Double *pVal); |
Interface |
IPowerLossSegment |