Contains the properties describing a segment of the power loss table used with a Power Meter as Receiver.
You can get a handle to one of these segments through PowerLossSegmentsPMAR.Item(n)
Example: Create a PMAR Device and Measurement
Methods |
|
---|---|
None |
|
Properties |
Description |
The frequency (Hz) associated with this segment. |
|
The loss value (dB) associated with this segment. |
|
Returns the number of this segment |
Interface |
Introduced with VNA Rev: |
IPowerLossSegment |
9.0 |