Write/Read
About Ext Pulse Gens

LowAmplitude Property


Description

Sets and returns the Low amplitude (voltage) of the pulse generator.

 VB Syntax

extPulseGen.LowAmplitude = value

Variable

(Type) - Description

extPulseGen

An ExternalPulseGenerator (object)

value

(Double) Pulse Generator low amplitude voltage.

Return Type

Double

Default

0

Examples

extPulseGen.LowAmplitude = 4 'Write

lo = extPulseGen.LowAmplitude 'Read

C++ Syntax

HRESULT get_LowAmplitude (double *pValue)

HRESULT put_LowAmplitude (double newVal)

Interface

IExternalPulseGenerator