Write/Read |
About LFE |
Description |
Enables/disables the low frequency extension (LFE). Learn more. |
VB Syntax |
chan.LowFrequencyExtension = value |
Variable |
(Type) - Description |
value |
(boolean) - Choose either: False - LFE is disabled. True - LFE is enabled. |
chan |
Channel (object) |
Return Type |
Boolean |
Default |
False |
Examples |
chan.LowFrequencyExtension = True 'Write |
lfestate = chan.LowFrequencyExtension 'Read |
|
C++ Syntax |
HRESULT get_LowFrequencyExtension(VARIANT_BOOL* lfestate); HRESULT put_LowFrequencyExtension(VARIANT_BOOL lfestate); |
Interface |
IChannel26 |