Write/Read | 
		About Integrated Pulsed App | 
	
Description | 
		Sets the pulse repetition frequency (PRF) for ALL internal pulse generators. This setting is equal to 1/period which is set with PrimaryPeriod Property Note: On the Pulse Setup dialog, this command is a "Basic" setting, intended to be used with the 'Auto' selections set to ON.  | 
	
VB Syntax | 
		pulse.PrimaryFrequency = value  | 
	
Variable | 
		(Type) - Description | 
	
pulse  | 
		A PulseMeasurementControl (object)  | 
	
value  | 
		(Double) PRF in Hz.  | 
	
Return Type | 
		Double  | 
	
Default | 
		1 kHz  | 
	
Examples | 
		pulse.PrimaryFrequency = 1e4 'Write  | 
	
value = pulse.PrimaryFrequency 'Read  | 
	|
C++ Syntax | 
		HRESULT get_PrimaryFrequency(double* value); HRESULT put_PrimaryFrequency(double value);  | 
	
Interface | 
		IPulseMeasurementControl2  |