Write/Read |
About SA Application |
Description |
Assigns a specified name to the Microsoft Windows shared data mechanism when MemShareEnabled is enabled. |
VB Syntax |
sa.dft.MemShareName = MemFileName |
Variable |
(Type) - Description |
sa.dft |
A SpectrumAnalyzerDFT (object) |
MemFileName |
(String) Memory file name. |
Return Type |
String |
Example |
sa.dft.MemShareName = "Mem_Share" 'Write |
name = sa.dft.MemShareName 'Read |
|
C++ Syntax |
HRESULT get_MemShareName(BSTR* MemFileName); HRESULT put_MemShareName(BSTR MemFileName); |
Interface |
ISpectrumAnalyzerDFT |