Write-only |
About SMC Phase |
Description |
Set the filename of the S2P file used to characterize the calibration mixer |
VB Syntax |
smc.MixerCharacterizationFile = value |
Variable |
(Type) - Description |
smc |
An SMCType (object) |
value |
(String) Full path, file name, and extension of the mixer characterization file. |
Return Type |
String |
Default |
Not applicable |
Example |
SMC.MixerCharacterizationFile = "C:\Program Files(x86)\Keysight\Network Analyzer\Documents\default.S2P" |
C++ Syntax |
HRESULT put_MixerCharacterizationFile(BSTR Value); |
Interface |
SMCType5 |