Write/Read
About SA Application

MultiToneDataDisplay Property


Description

Sets and returns the data display mode.

 VB Syntax

sa.coherence.MultiToneDataDisplay = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(enum NASACoherentDataDisplay) - Choose from:

0  naSAShowAll: Legacy SA mode - all frequency points are displayed.

1  naSAZeroNonTones: All the frequencies that are not on the multi-tone coherence grid are set to 200 dBm before being displayed.

Return Type

Enum as NASACoherentDataDisplay

Default

naSAShowAll

Examples

sa.coherence.MultiToneDataDisplay = naSAShowAll 'Write

DisplayMode = sa.coherence.MultiToneDataDisplay 'Read

C++ Syntax

HRESULT get_MultiToneDataDisplay(tagNASACoherentDataDisplay* value)
HRESULT put_MultiToneDataDisplay(tagNASACoherentDataDisplay value)

Interface

ICoherenceSA