Write/Read
About SA Application

MultiToneHarmonicRejection Property


Description

Sets and returns the number of test signal harmonics you want to be protected against. This adds constraints to the list of LOs used to cover the span.

VB Syntax

sa.coherence.MultiToneHarmonicRejection = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Long)  Number of test signal harmonics to be protected. The more this number is increased, the more constraints are added on the span LOs setting.

Return Type

Long

Default

0

Examples

sa.coherence.MultiToneHarmonicRejection = 0  'Write

value = sa.coherence.MultiToneHarmonicRejection 'Read

C++ Syntax

HRESULT put_MultiToneHarmonicRejection(long value);

HRESULT get_MultiToneHarmonicRejection(long* value);

Interface

ICoherenceSA