Write/Read
About SA Application

MultiTonePeriod Property


Description

Sets and returns the test signal repetition rate (in seconds). This value is 1/MultiToneImageRejectSpacing.

VB Syntax

sa.coherence.MultiTonePeriod = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Double)  Test signal repetition rate (in seconds)

Return Type

Double

Default

1E6

Examples

sa.coherence.MultiTonePeriod = 1E6  'Write

value = sa.coherence.MultiTonePeriod 'Read

C++ Syntax

HRESULT put_MultiTonePeriod(double freqval);

HRESULT get_MultiTonePeriod(double* freqval);

Interface

ICoherenceSA