Write/Read |
About Noise Figure |
Description |
Sets and reads the gain state of the noise receiver. This setting is NOT used when NoiseReceiver = naStandardReceiver (Opt 028) |
VB Syntax |
noise.NoiseGain = value |
Variable |
(Type) - Description |
noise |
A NoiseFigure (object) |
value |
(long integer) - Gain value. Choose from: 0 Low Gain select if the gain of your DUT is relatively high (>35 dB). 15 Medium Gain select if the gain of your DUT is about average (20 dB to 45 dB). 30 High Gain ..select if the gain of your DUT is relatively low (<30 dB). If the value does not match one of these, it is rounded up to the next legal value. |
Return Type |
Long Integer |
Default |
30 |
Examples |
noise.NoiseGain = 30 'Write |
GainNoise = noise.NoiseGain 'Read |
|
C++ Syntax |
HRESULT get_NoiseGain(long* pVal) HRESULT put_NoiseGain(long newVal) |
Interface |
INoiseFigure |