Write/Read
About Mixer Configuration

NominalIncidentPowerState Property


Description

Toggles the Nominal Incident Power setting ON and OFF. This setting is ONLY to be used with SMC measurements, not VMC. Learn more about Nominal Incident Power.

 VB Syntax

mixer.NominalIncidentPowerState = bool

Variable

(Type) - Description

mixer

A Mixer  (object)

bool

(boolean) - Nominal Incident Power State. Choose from:

1 -(True) Turn nominal incident power ON

0 -(False) Turn nominal incident power OFF

Return Type

Boolean

Default

0 -(False)

Examples

mixer.NominalIncidentPowerState = True 'sets NominalIncidentPowerState to ON

C++ Syntax

HRESULT get_NominalIncidentPowerState(VARIANT_BOOL *pVal)

HRESULT put_NominalIncidentPowerState(VARIANT_BOOL val );

Interface

IMixer4