Write/Read
About Independent Power Calibration

NumberOfPoints (PowerCalRange) Property


Description

Sets and gets the number of points for range <m> for source port<n>. 

 VB Syntax

PwrrCalRange.NumberOfPoints = points

Variable

(Type) - Description

points

(Long) - Variable to store the returned number of points.

PwrrCalRange

A PowerCalRange (object)

Return Type

Long

Default

Not Applicable

Example

CalibrateAllChannels.IndependentPowerCalibration(3).PowerCalRange(1).NumberOfPoints = 7 'Write

points = CalibrateAllChannels.IndependentPowerCalibration(3).PowerCalRange(1).NumberOfPoints 'Read

C++ Syntax

HRESULT get_NumberOfPoints(long* points);

HRESULT put_NumberOfPoints(long points);

Interface

IPowerCalRange