Read/Write |
|
Description |
This command is replaced with SetIsolationPaths and GetIsolationPaths. Sets and returns whether Isolation portion of the calibration will be performed or not. |
VB Syntax |
obj.OmitIsolation = bool |
Variable |
(Type) - Description |
obj |
SMCType (object) or VMCType (object) |
bool |
(Boolean) True - Isolation is NOT performed False - Isolation is performed |
Return Type |
Boolean |
Default |
True |
Examples |
value = SMC.OmitIsolation |
C++ Syntax |
HRESULT put_OmitIsolation (VARIANT_BOOL bState) |
Interface |
SMCType VMCType |