Read-only
About PNOP / PSAT Marker Search

POut Property


Description

Returns the POut result of the PNOP or PSAT marker search.

PSAT Out = Marker 2 Y-axis value

PNOPOut = Marker 4 Y-axis value

 VB Syntax

pOut = pMark.POut

Variable

(Type) - Description

pOut

(double) - Variable to store returned value

pMark

A PNOP (Object) or PSaturation (Object)

Return Type

Double

Default

Not applicable

Examples

pOut = pMark.POut 'Read

See example program

C++ Syntax

HRESULT get_POut(double* pNewVal)

Interface

IPNOP or IPSaturation