Write/Read
About Marker Search

PeakThreshold Property


Description

Sets peak threshold for the specified marker. If a peak (using the criteria set with PeakExcursion) is below this reference value, it will not be considered when searching for peaks.

 VB Syntax

mark.PeakThreshold = value

Variable

(Type) - Description

mark

A Marker (object)

value

(single) - Peak Threshold. Choose any number between:
-500
and 500

Return Type

Single

Default

-100db

Examples

mark.PeakThreshold = 1 'Write

PkThresh = mark.PeakThreshold 'Read

C++ Syntax

HRESULT get_PeakThreshold(float *pVal)
HRESULT put_PeakThreshold(float newVal)

Interface

IMarker