Write/Read |
About Phase Control |
Description |
Write and read whether to use the phase correction offset array. Use PhaseCorrectionData to write or read the offset data. |
VB Syntax |
phase.PhaseCorrectionEnabled(srcPort) = value |
Variable |
(Type) - Description |
phase |
A PhaseControl Object |
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Boolean) Phase correction array state. True – Apply phase correction offset array. False – Do NOT apply phase correction offset array. |
Return Type |
Boolean |
Default |
False |
Examples |
phase.PhaseCorrectionEnabled 1 = True ' Write |
value = phase.PhaseCorrectionEnabled 2' Read |
|
C++ Syntax |
HRESULT get_PhaseCorrectionEnabled(long port, VARIANT_BOOL* pVal); HRESULT put_PhaseCorrectionEnabled(long port, VARIANT_BOOL newVal); |
Interface |
IPhaseControl |