Write/Read |
About Phase Control |
Description |
Write and read the ratioed receivers (parameter) and paired port to use for phase control. |
VB Syntax |
phase.PhaseParameter(srcPort) = value |
Variable |
(Type) - Description |
phase |
A PhaseControl Object |
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(String) Ratioed parameter. Choose any two VNA physical receivers. Use either standard receiver notation ("R/R3") or logical receiver notation ("a1/a3"). Separate the two receiver names by a forward slash '/'. For example: "a1/a3". |
Return Type |
String |
Default |
"a1/b1" |
Examples |
phase.PhaseParameter 1 = "a1/a3" ' Write |
value = phase.PhaseParameter 2' Read |
|
C++ Syntax |
HRESULT get_PhaseParameter(long port, BSTR* pVal); HRESULT put_PhaseParameter(long port, BSTR newVal); |
Interface |
IPhaseControl |