Write/Read |
About Phase Coherent Measurements |
Description |
Enables/disables phase computing. |
VB Syntax |
sa.coherence.PhaseProcessState = value |
Variable |
(Type) - Description |
sa.coherence |
A SpectrumAnalyzerCoherence (object) |
value |
(Boolean) Choose from: 0 - OFF - Phase computing disabled. 1 - ON - Phase computing enabled. |
Return Type |
Boolean |
Default |
OFF |
Examples |
sa.coherence.PhaseProcessState = ON 'Write |
value = sa.coherence.PhaseProcessState 'Read |
|
C++ Syntax |
HRESULT get_PhaseProcessState(VARIANT_BOOL*
enable) |
Interface |
ICoherenceSA2 |