Write/Read
About Active Match

PhaseSweepPoints Property


Description

Set and read the number of phase points. For the tuning tone at the output, a phase sweep is done for each point.

 VB Syntax

HotS22.PhaseSweepPoints = value

Variable

(Type) - Description

HotS22

A ActiveParametersApp (object)

value

(Long) - Number of phase points. Do not exceed the max number of phase points (50).

Return Type

Long

Default

8

Examples

HotS22.PhaseSweepPoints = 201 'Write

value = HotS22.PhaseSweepPoints 'Read

C++ Syntax

HRESULT get_PhaseSweepPoints(long* value)

HRESULT put_PhaseSweepPoints(long value)

Interface

IActiveChannelSettings