Write/Read
About Phase Offset

PhaseOffset Property


Description

Sets the Phase Offset for the active channel.

 VB Syntax

meas.PhaseOffset = value

Variable

(Type) - Description

meas

A Measurement (object)

value

(double) - PhaseOffset in degrees. Choose any number between:
 
-360 and +360

Return Type

Double

Default

0

Examples

meas.PhaseOffset = 25 'Write

poffset = meas.PhaseOffset 'Read

C++ Syntax

HRESULT get_PhaseOffset(double *pVal)
HRESULT put_PhaseOffset(double newVal)

Interface

IMeasurement