Write/Read |
About PointSweep |
Description |
Turns point sweep ON or OFF for all measurements on the channel. Point sweep measures both the forward and reverse parameters at each frequency point before stepping to the next frequency. The display trace is updated after the forward and reverse parameters are measured at that frequency point. |
VB Syntax |
chan.PointSweepState = state |
Variable |
(Type) - Description |
chan |
A Channel (object) |
state |
(boolean) False - Turns point sweep OFF True - Turns point sweep ON |
Return Type |
Boolean |
Default |
False |
Examples |
chan.PointSweepState = True 'Write |
averg = chan.PointSweepState 'Read |
|
C++ Syntax |
HRESULT get_PointSweepState(VARIANT_BOOL *pVal) |
Interface |
IChannel16 |