Read-only |
About External Testset Control |
Description |
Returns a comma-separated list of the Output port selections that are available for a given logical input port. Read the number of input ports for the test set using NumberOfPorts Property. |
VB Syntax |
value = tset.PortCatalog(logPort) |
Variable |
(Type) - Description |
value |
(String) Variable to store the returned information. |
tset |
A TestsetControl object. |
logPort |
(Long) Logical Input port number for which to return valid output ports. |
Return Type |
String |
Default |
Not Applicable |
Examples |
value = testset1.PortCatalog 2 |
C++ Syntax |
HRESULT get_PortCatalog(long inputPort, BSTR *outPort); |
Interface |
ITestsetControl |